AXIS#.BODE.VAMP
Description
AXIS#.BODE.VAMP sets the amplitude of the excitation when in velocity mode as set in AXIS#.BODE.INJECTPOINT.
Example
Code
Set the excitation velocity to 100 RPM
"Revolutions per minute"
Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component:
--> AXIS1.BODE.VAMP 100
Get the excitation velocity (already set to 100 RPM):
--> AXIS1.BODE.VAMP
100.000 [rpm]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
0 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.BODE.VAMP | 0x5001 | 0x3 | DINT | - | Velocity | RW | False |
| AXIS2.BODE.VAMP | 0x5101 | 0x3 | DINT | - | Velocity | RW | False |